This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867 - WoL and Magnetics



Hi,


We intend to use the DP83867 but have the following questions which are not discussed in the datasheet.

1. WoL Feature

The RevC Datasheet states: "Wake on LAN provides a mechanism for bringing the DP83867 out of a low-power state using a special Ethernet
packet..."

Please specify which of the 4 available low-power modes can be utilized together with WoL.

2. Magnetics

We need a transformer which a PCMCIA form factor. Pulse has a variety of PCMCIA-size 1Gb transformers but which one would be suitable for the DP83867?

Thanks and Regards,

Fred