It is possible that TFP410 DVI outputs connect to other DVI outputs because one DVI connector can connect to other DVI connector. Can this case cause permanent damage to the TFP410?
The latch-up current in the Absolute Maximum Ratings is 100 mA. Can above case cause the latch-up?
Range of the external DVI single-ended termination resistance (RT) in the Absolute Maximum Ratings is 0 ohm to open circuit. Does this mean that the output terminal can directly connect to GND?
Best regards,
Daisuke