Other Parts Discussed in Thread: ALP
I need to open ALP tool and select the serializer connected with the PC automatically .
I have tried the following VBA script in excel
Sub Initialization()
Shell ("C:/AnalogLaunchPADv1.54.0010/MainGUI.exe")
End Sub
But it throws a error like
Traceback (most recent call last):
File "MainGUI.py", line 28, in ?
ImportError: No module named Strings.
Same i have tried with the following python code
import os
import subprocess, sys
from subprocess import Popen, PIPE
subprocess.Popen(r"C:/AnalogLaunchPADv1.54.0010/MainGUI.exe")
Same error thrown after executing the python script.
Traceback (most recent call last):
File "MainGUI.py", line 28, in ?
ImportError: No module named Strings.
But if I open the MainGUI.exe directly it is opening properly without any error.
Can you please tell how to open the ALP tool and select serializer connected automatically through VBA or Python script .
Quick response is most appreciable.
Thanks,
Jaisshri.C