Other Parts Discussed in Thread: SN65HVD05
Having ridiculous intermittent problems controlling
St-30 RS485 Somfy part #1000658 I have a Crestron processor AV2 sending out RS-485 to 44 somfy shade motors in less than a 4000 ft wired network using cresnet wire for power and communication. 4 ten port somfy module boards and one 5 port somfy module board. I put a 10k ohm resister in the last open port. Terrible intermittent problem. Somfy claims they can handle 255 RS-485 motors on less than 4000 ft wired network. I can't control 44 motors without problems. I am looking at your part: Will this have any affect? Also is there a problem with Somfy's understanding of Nodes what actually their motor network will work for RS-485 commands? Thanks,
SN65HVD05 (ACTIVE)
High-Output RS-485 Transceiver