Other Parts Discussed in Thread: AM26LS32AC, AM26LV32, AM26LV32E, LSF0204, 74ACT11032
Dear members!
I will desing RS-422 Driver for encoder interface using AM26LS32AC but am faced with a problem related to I/O Level between AM26LS32AC and processor.
Q1) Voltage level sifter between AM26LS32AC and processor
Vout of AM26LS32AC is 2.5~2.7[V] but Vout-Max is over 3.3[V] by using conditions.
I think that it add Voltage level shift LDS0204 between processor and AM26LS32AC.
LDS0204 didn't mention the range for VIN,VOUT related to port and mentioned the range for EN Pin.
Please review the block diagram above.
Q2) I know that termination resistor is using 80~120[ohm] between Plus and negative line for AM26LS32.
Because of differntial line voltage, I think that the general analog switch can apply to AM26LS32 differential line
Could you recommend the suitalble analog switch to change Max14761 that support +/-15V
Thanks