Other Parts Discussed in Thread: DS90LV011A, DS90LV012A, DS90LT012A
Hi,
We have signals being transmitted between circuit cards with DS90LV011AQ LVDS differential drivers and DS90LT012AQ LVDS differential receivers. On the receiver side we have fail safe biasing resistors installed consisting of a 2 kΩ from the positive input to the +3.3 V supply and a 2 kΩ from the negative input to common ground. For the purpose of failure mode effects analysis, in the event one of these biasing resistors were to fail open would the receiver still be able to decode transmissions from the driver? The receiver and driver have separate 3.3 V power supplies connected to the same common ground, so there should be very little ground potential difference.
Page 4 of the receiver data sheet indicates signals greater than 100 mV can be detected over a ±1V common mode range centered around the +1.2 V driver offset voltage. From the driver datasheet, it is not clear how strong the driver offset voltage is? In the event of an open fail safe bias resistor, would the remaining 2 kΩ resistor be strong enough to pull the offset voltage outside the 1.2±1 V region?
Regards,
Jesse