Hello,
Is 5V @ 5A a possible negotiated power setting for PP_EXT with TPS65982?
Looking at the USB PD spec, it would seem that a DFP advertising Profile 5 (capable of supplying at least 5V @ 2.0A, 12V and 20V at 5A respectively) would be able to negotiate a current increase to 5A without a voltage increase. However, I'm not clear whether this is actually possible - looking at Table 2 in the latest EVM User's Guide, a 5V@5A sink is unsupported by any of the built-in EVM profile examples.
Thanks,
Jonathan