This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB940 operation mode



Hi, TI, Customer want to use the device in "1 lane FPD-Link III Input, 2 MIPI lanes Output" mode. Please let me know the coufiguration of the device with Table 7 and 8.      Is it OK to set the device as #3 config of Table 7 ? Under this mode, is it possible to set the device as #1 config of Table 8 ? (Customer want to use STP and 400KHz I2C on BC.) Any way , The device has alot of "mode". Please let us know the meaning of   1. "MODE" in Table 7 2. "CSI LANE" in Table 7 3. "CSI SEL" in Table 8 4. "MODE" in Table 8
  • Hi TI, Could you please answer the questions ?
  • Could you please answer the quewtions ?
  • Hi Toshi,

    Yes, you can use Mode #3 for MODE_SEL0 (Table 7). If you look at the 3 columns of Mode, CSI Lane, and Replicate, they form the 3 bit decode of this analog input. It ranges from 000 to 111, and the last column of Output Mode describes what each row means.

    The Mode column for MODE_SEL1 (Table 8) is similar, it just pairs with the CSI_SEL column to show the 3 bit decode. Mode #1 in this table corresponds to CSI port 0 being active, 5Mbps back channel rate, and STP cable. If that matches the customer application, then this mode is correct.

    Thanks,
    Jason