I'm using a DP83848CVV, with a POE circuit, and a When it works it works very well, and i have no problems. However from time to time the PHY dies.. Replacing it fixes the problem... With non POE stuff they are rock soild. I've put TVS diodes across the Line side of the transformer and that helped.
I'm now thinking i shoudl put TVS didodes on both sides of the Transformer, so i can protect against both differential and common mode issues.
What else can i do to make things more reliable.
Is there a more roubust PHy?