Other Parts Discussed in Thread: TRS3221
How to combine RS232 and RS485 communication through to wires in one circuit design? It should be software configurable.
I've to delvelop a device which should communicate over a two wire connection either with a RS232 or with a RS485 protocol. I've following questions:
I've seen the "RS-485 / RS-232 Multiprotocol Transceiver Reference Design". Is it possible to use this solution for a two wire Connection?
If not, I want to ask following questions:
1) How can I design a circuit which is able to switch 120 Ohm Termination resistor in a transmission line?
2) Which RS232 transmitters are able to go in high impedance state if they are shuted down?
3) Which RS485 transmitters are able to go in high impedance state if they are shuted down?
3b) Which RS485 transimitters are able to switch a termination resister internal, too?
4) Are there other better aproaches?
Best regards
Walter Kotz
Austria