Other Parts Discussed in Thread: TUSB321AI
In the TUSB321AI datasheet it says the voltage on the CC1, CC2 pins cannot exceed VDD + 0.3V. What happens if you connect an un-powered DFP interface (VDD = 0V) to a powered downstream DFP interface that could have Rp pullups tied to 5V on their CC lines (or are the CC lines protected from this in ways not discussed in the datasheet?)