Other Parts Discussed in Thread: TMDS442, HD3SS215
We are trying to find a way to evaluate the TMDS442 in a specific application, but we can not find it on an eval board. Is his device on any eval boards which provide access to the TMDS442?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tricia,
Unfortunately we don't have evaluation modules for TMDS442.
If useful, I can send you a reference schematic.
Regards
Is there a similar chip that does have an eval board.
I'm looking to make a simple PiP module. 2 HDMI signals to SideBySide or TopBottom single hdmi. Input and Output 1080P, 60Hz, 120Hz would be the best.
If I am going to have to make a board myself, are they avail in something bigger than surface mount? Lol. My hands aren't as steady as they used to be.
Hi Aaron,
The TMDS442 is an active crosspoint switch 4:2 for HDMI supporting data rates up to 2.25Gbps.
We have HD3SS215, this is a passive switch 2:1 for HDMI2.0 supporting data rates up to 6Gbps. This device has an EVM available for order on ti.com
Regards