Other Parts Discussed in Thread: TUSB211
Hi all
Would you mind if we ask TUSB211?
<Question1>
Our customer would like to use USB2.0 with using 10m cable.
So, we heard from you that it is required two TUSB211 as the redriver.
In this case, how much of EQ gain settinng should we choice(from Level0 to Level3)?
Of course, we recognize that it depends on the cable length.
If you have some experience about it, could you let us know?
<Question2>
On the datasheet P8, why does C4 require?- Only for the delay, for noise?
<Question3>
The max cable length of USB2.0 is 5m.
So, if the cable length is less than 5.0m, it is not required to add TUSB211 for redriver, is it?
Kind regards,
Hirotaka Matsumoto