We have multiple usb 2.0 cameras plugged into a usb 2 hub but are having bandwidth problems between the hub and host. Are the any usb 3 hubs that will transmit that usb 2 data over the usb 3 link, or do they all go into their own usb 2 and 3 hubs? For example, the TUSB8040A1 explicitly shows four usb 2 ports going into the internal hub and out on a usb 2 port, similarly for the four usb 3 ports.
Thanks