This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using DS90Ux949 eval kit, problem with getting image



I was using an older laptop, Windows 7, Extend mode, NVidia chipset and was able to get an image out of my 948 eval kit (connected to the 949 eval kit).

However:

New Dell laptop, Windows 10, Intel chipset, duplicate mode (extend mode didn't allow correct resolution), laptop display at 1920 x 1208, both LED indicators on 949 board are on (RX_5V and HPD), I get no image out of my 948 board.

Is there a windows driver I need to get to update this new laptop?

Thank you