Other Parts Discussed in Thread: SN75DP130, TCA9517
I Have a customer, he is using the SN75DP130 for a DP sink(Rx) with FPGA.
My questions is that can I use DP130 without programming through I2C?
Because my customer schematic had wrong interface circuit of SCL_CTRL and SDA_CTRL between the DP130 and FPGA.
I2C signals direct connected of two devices pins, but those IOs standard are mismatch, DP130(3.3Volt) FPGA(1.8Volt). I think that he doesn’t use I2C interface.
If I use DP130 device for re-driver to bring DP Sink mode when don't use two signals of SCL_CTRL and SDA_CTRL.
Can someone recommended a workaround solution to use in this manner?