Other Parts Discussed in Thread: TPD12S520, TPD1E05U06, TS5A3166
Hi,
We are using the ESD protection & level shifting device - TPD12S520 in the HDMI input path of one of our boards. We have done the TPD12S520 design as per the receiver side application schematic provided in the datasheet (snapshot provided below for reference). Note that we have used LV supply of 3.3V.
Here the HPD_OUT (hot plug detect) pin of TPD12S520 is pulled-up to 5V HDMI using 1k resistor near the HDMI connector. So as soon as the HDMI source is connected, the HPD will be asserted (driven high) to the source. This will happen even if the board is powered OFF.
This condition is creating issues in our testing and results in the video standard change of the HDMI source. So to avoid this problem, we are planning to remove the 1k pull-up resistor on the HPD pin at the connector side and also change the 100k pull-up to 1k on the HPD_IN pin on the HDMI receiver IC side.Note that as per the HDMI specifications, the source should have around 10K pull-down on the HPD input.
By doing these changes, the HPD output will be low when the source is connected with board powered OFF and will be asserted only when the HDMI receiver IC is powered ON & active.
Kindly let us know if these changes can be made in the TPD12S520 schematic.
Regards,
Elvin