Other Parts Discussed in Thread: DS30EA101, DS90UB928Q, DS30BA101
DS30EA101 datasheet describes in the AC Electrical Characteristics the total jitter and the test conditions. When 75ohm coaxial cable (RG59) is used, it seems the cable length can be up to 100 meters at 3.125 Gbps.
In this test condition, What is the maximum cable loss? Are there the details of the cable specification?
Our customer is using the coaxial cable of 60 meters and connecting DS90UB925Q and DS90UB928Q via DS30BA101 and DS30EA101, but there are errors in the video output. If the total jitter between DS30BA101 and DS30EA101 is 0.3UI, the jitter should not be a cause of the errors because the DS90UB928Q has the jitter tolerance of approximately 0.6UI. When the DS90UB928Q is set to LCBL mode that affects the input adaptive equalizer (AEQ), the errors seem to be improved.
I am concerned that the cable quality is bad. About the relationship between the cable length, the data rates, the cable loss or jitter, are there the test results for the cables of various grade?
Best regards,
Daisuke