Other Parts Discussed in Thread: SN75DP130
Hi Team,
As SN75DP130 application note mention, in a sink application, it is better to set DP130 and not to work in a default mode. my question is below.
1. when link trainning is disable and I2C control is enable, if need to set output VOD and Pre-emphasis first, then set up input Equalize? The PE level define the max
Equalize dB for each lane?
2. in order to get the best eye result, how to define output VOD and Pre-emphasis level in sink appliction when link trainning disable? It is decided by trace length
from DP130 to FPGA?
3. I meet the case that when set input Equalize dB first, then set up output VOD and Pre-emphasis, the chip will swithc off. Is it normal?
4. for DP130 output eye result, if the eye height is improved but in sacrifice of eye width?
5. what is the meaning of the yellow words? if it mean when I2C control enable and link trainning disalbe, Pre-emphasis should be L1?
5.