Other Parts Discussed in Thread: BQ24392, BQ24392EVM, BQ24192
Hi,
I consider to use the BQ24392 charger detector on my PCB. I purchased the BQ24392EVM and the TPS2546EVM (charger controller) to test it. unfortunately the detector doesn't seems to work - does not recognize the various charging modes of the controller. the setup is as follows:
The controller 5V VSUB voltage is supplied by a lab PS which can drive up to 4A. Its input USB port connected to a PC with a 1m standard USB cable without its VSUB wire (I disconnected it). The ILIM and EN jumpers are not populated. the CTL jumpers are populated in different combinations according to Table 4 in the datasheet.
The controller USB Out is connected to the detector USB In by a 1m USB3 cable.
The controller microUSB Out is connected to an Android smartphone (Nexus 5).
The controller DM_OUT and DP_OUT TPs are connected to a scope (When I turns the power supply ON I can see clearly these signals voltage changes dynamically and differently according to the above jumpers combinations).
The detector CHG_AL_N and SW_OPEN LEDs lit and CHG_DET LED is off a second after power-on. The problem is that this is the same and only status of the LEDs independent to the controller jumpers configuration.
Can anybody tell what can be the reason for this miss detection?
Thanks,
Shony