This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867CR as RGMII mode

Guru 10265 points

Other Parts Discussed in Thread: DP83867CR


Hi all,

My understanding is when I use DP83867CR as RGMII mode,
RX_D4-7 and RX_ER, COL, CRS cannot be assigned to SFD mode.
Is it correct?

From Datasheet(Page-9):

RX_D4_7 : RECIEVE DATA Bit 4: This signal carries data from the PHY to the MAC in GMII mode.

RX_ER / GPIO: ... In RGMII, the RX_ER pin is not used

COL / GPIO: ... In RGMII, the RX_ER pin is not used

CRS: ... In RGMII, the RX_ER pin is not used

http://www.tij.co.jp/jp/lit/ds/symlink/dp83867cr.pdf


Best regards,
Kanae