Hi,
I think I damaged the chip when the chip on the board was not powered up an was driven by an LVDS driver. Now there is a 3.3 volt to ground short on the board.
Ken
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I think I damaged the chip when the chip on the board was not powered up an was driven by an LVDS driver. Now there is a 3.3 volt to ground short on the board.
Ken
Hi Ken,
This sounds more like an ESD or Electrical overstress event. The DS90LV047A is an LVDS driver. do you have multiple LVDS drivers connected together. the LVDS outputs of the DS90LV047A are designed to handle voltages up to 3.6V when VCC = GND = 0V.
Regards,
Lee