This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Magnetics Integrated IP67 Rated Connector for Ethernet

Hello TI Ethernet!

I am looking for a connector that has integrated magnetics that complies with the IP67 standard for 10/100 Ethernet.

Do you have any recommendations?

Thanks,

Eric Dahl

  • Hi Eric,

    It isn't common to find IP67 RJ45 jacks with integrated magnetics, and it will offer greater design flexibility to have a discrete magnetics setup.

    I was able to locate an integrated magnetics module from Metz Connect P/N: MJT5213111 but not much else.

    Best Regards,