I am looking for Single channel RS232 Line driver / receiver IC which shall have following feature
- support 1Mbps data rate
- Shall have inbuilt Short circuit protection
- ESD protection ( +/-15kV HBM)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am looking for Single channel RS232 Line driver / receiver IC which shall have following feature
Shamanth,
There many versions of two basic device pin outs.
The pin outs are 3221 and 3227. 3221 receiver EN pin and 3227 has driver READY output. 3221 is auto power down and 3227 is auto power down plus.
15k HBM ESD plus IEC 61000-4-2 on some.