Hi,
I have a customer who is looking for is a SATA re-driver that can drive an eSATA port. The customer's current design has 4 SATA connections coming from a uProcessor to 3 eSATA connectors as well as a one CFast connector. They have built a board up and this arrangement doesn’t quite make it for SATA3 speeds which are 6Gbps and the customer believes a re-driver is needed. Is the SN75LVCP601 the best choice or is there a better recommendation we should be considering?
Thanks,
PSB