Other Parts Discussed in Thread: LMH1983
Hi all ,
On my board I have a LMH1983 for normal SDI video locking. I'm using the default loop filter from the data sheet.
I now want to reuse this board to lock to an HSync which is derived from an IEEE1588 clock. This Hsync is filtered but still makes steps of +/- 6ns since the clock which generates this pulse is using 156.25MHz as a base clock. For this I'm not using the VSync or FSync pulses, just HSync. Therefore I'm not relying on TOF pulses, just using the 148.5MHz
When doing this, the PLL1 never locks. PLL2 and PLL3 are indicating lock. I disabled crash-locking. My question is, Is the 6ns jitter on the HSync pulse to high for PLL1 to remain in lock? This is less then a 27Mhz clock period.
As a fallback scenario I had the I2C interface in mind to control the DAC immediately but these steps are not accurate enough to remain within SDI jitter spec. Correct or am I missing something?
William