http://videosolutions.ltd.uk/tech-articles/ULPI%20interface.html
Is SOF the first packet that is observed after device initialization [i.e. after chirp, squelch, not squelch]? Will the SOF packets continue as long as USB link is maintained? We receive SOF after 50oddms of initialization in windows 8 and 12 ms odd in windows 7. Is it normal behaviour? Shouldn't the device phy be reset observing no activity for 50 /12 ms after initialization?
When does this second device reset comes from the HOST or does it ever come? If so then how do we detect it and will it again cause chirping etc? Again will the SETADDRESS command will follow the second device reset?