This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0366 signal detect control



Hi, TI, I'd like to confirm the Signal Detect Reset(Add:0x20h, bit :6 ) function. I've found that when I save "0" to the Signal Detect Reset(Add:0x20h, bit :6 ), then the LOCK_DET(add:0x01 , Bit:4) will be "0" also. Is this a spec of the device ?