This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0366 Signal detect question



Hi, TI. I have a question of Signal detect function, If the input signal was changed from signal A to Signal B( A and B are same rate and same phase but different movi, I guess the device will not into unlock state ), Does the "Signal detect function" can detect the change of the signal(The bit of SIG_DET cnaged as "1 -> 0 -> 1") ? or cannot detect the change(The bit of SIG_DET always "1") ?