Other Parts Discussed in Thread: SN75ALS172, SN75ALS172A
Dear Technical Support Team,
What the difference between SN75ALS172 and SN75ALS172A.
SN75ALS172 is already nothing on TI website.
Best Regards,
y.i
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN75ALS172, SN75ALS172A
Dear Technical Support Team,
What the difference between SN75ALS172 and SN75ALS172A.
SN75ALS172 is already nothing on TI website.
Best Regards,
y.i
These are the specifications that are different on SN75ALS172DWR
Pinout for DIP package is the same, however pinout for DW package is NOT same.
SN75ALS172
DC Parameters:
IIL = (When VI = 0.5V) -360µA Max
IOS = (When VO = -7V to 12V) 500mA max.
ICC = (With no load and Outputs enabled) typical is 38 mA and max is 60mA.
ICC = (With no load and Outputs disabled) typical is 18mA and max is 40mA.
AC Switching Parameters:
td(OD) Differential-output delay time = (With a RLoad of 54 ohms) typical 45ns and max is 65ns.
tt(OD) Differential-output transition time = (With a RLoad of 110 ohms) typical 80ns and max is 120ns.
tPZH Output enable time to high level = (With a RLoad of 110 ohms) typical 80ns and max is 120ns.
tPZL Output enable time to low level = (With a RLoad of 110 ohms) typical 45ns and max is 80ns.
tPHZ Output disable time from high level = (With a RLoad of 110 ohms) typical 78ns and max is 115ns.
tPLZ Output disable time from low level = (With a RLoad of 110 ohms) typical 18ns and max is 30ns.