This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

device to replace a WIFI module by Ethernet phy with SDIO interface?

Hi,

I have a design with a WIFI module. The interface between the processor and the WIFI module is a SDIO V2.0 interface.

But, I need to change the WIFI by Ethernet... So I'm looking for a solution (1 or 2 or 3 devices) to make this modification.

The dificulty is to get an ethernet PHY with a SDIO interface, I haven't MII or RMII or SNI (I think those interfaces are not compatible with SDIO).

The SDIO interface is with the pins SDIO_DATA[0..3], SDIO_CMD and SDIO_CLK.

Have you a solution?

Thanks for your help.