Other Parts Discussed in Thread: TPD4E001
Using TPD4E001DRL in a circuit where it is covered by an epoxy material (Loctite 3364). This is a Urethane Adhesive/Potting Compound. In this design the power pin is not connected and 2 of the signal pins are connected to analog outputs (0-5V). The ground pin is connected to ground and the other 2 signal pins are not connected. The issue we are having is that in a few cases a low resistance (80 ohms - 1K ohm) is developing between one of the connected signal pins and ground pin. At this point we have not been able to remove the potting compound to get at this part to examine it more closely. Is there a failure mode for this part where such a low resistance to Gnd pin could be created internally? Have there been any problems reported using this part with a potting compound?