Other Parts Discussed in Thread: DS16EV5110A, DS16EV5110, DS15BR400, DS25BR400, DS42BR400, DS100BR410
Hi, folks
I can not find any description Clock&data re-sync circuitry for DS16EV5110A.
Can we use DS16EV5110A for 4 channel individual redrivers?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS16EV5110A, DS16EV5110, DS15BR400, DS25BR400, DS42BR400, DS100BR410
Hi, folks
I can not find any description Clock&data re-sync circuitry for DS16EV5110A.
Can we use DS16EV5110A for 4 channel individual redrivers?
Hi Kajino-san,
The DS16EV5110 is specifically designed for a 3-data + 1-clock application. Four channel redrivers are common at datarates from 1.5 - 10+ Gbps. Here are some examples.
1.5 Gbps - DS15BR400
2.5 Gbps - DS25BR400
4.0 Gbps - DS42BR400
10 Gbps - DS100BR410
Regards,
Lee
Hi,
You are correct there is no internal mechanism to provide a "zero delay output". In addition to the DS16EV5110A all of the buffers mentioned do have a finite propagation delay. The relationship between clock and data is maintained from input to output due to the very low skew from one channel to the others.
Best Regards,
Lee