This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220 Vbus_Det pin issue

Hi Team

VBUS_DET IO Pin : The threshold range is 2.95V to 3.8V.

The Vbus_Det need  One 900K external resistor required between system VBUS and VBUS_DET pin.

But SPEC have Show : Internal pull-down resistor ( 95k ohm ) at VBUS_DET pin

So 95kohm and 900k ohm will be divisional.

Vbus = 5V ==> Vbus_Det = 0.43V

Vbus = 28V ==> Vbus_Det = 2.4V

Could you help to Explanation Why we need put 900k ohm on this pin?