Dear Sir,
We have some queries related to FPD link III chip sets:
If the COTS modules uses DS90UB913A-Q1 (10/12-Bit FPD-Link III SERIALIZER) , can we use DS90UH926QSQ/NOPB (5 - 85 MHz 24-bit Color FPD-Link III Deserializer with HDCP) at our design for deserializing , the FPD link III data ?
Similarly can we use DS90UH925QSQ/NOPB (SERIALIZER)in our design for interfacing ( FPD link III ) to COTS system which uses DS90UB914A-Q1(Deserializer).
Kindly do the needful at the confirm at the earliest possible.
Thank you in advance and Best Regards,
Sanjay