Other Parts Discussed in Thread: DS15BA101
Hi,
I have a PCB design where an FPGA (Zynq) drive the DS15BA101 directly.
Because of the absolute maximum ratings of the DS15BA101 the FPGA drive IN+ and IN- of the DS15BA101 with 3,3V and GND.
But when I measure the voltages on the Outputs both are at about 1V. There is no difference if I toggle the input or if it's driven with DC voltage.
Have somebody any idea what I can try next to figure out where the problem is?
RVO is 953Ohm
OUT+ and Out- have each a 49,9Ohm Pull-Ups and a 1uF serial capacitor.
Thanks a lot,
Martin