This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO154X two battery I2C isolation



I am designing a Smart Battery fuel gauge and I was wondering if the following is possible with the ISO154X:

I have two cells inside the Smart battery pack, with two I2C ports referenced to two grounds depicted in the picture. I want to use both I2C ports but since the signals are referenced to different grounds I can't read the two ports. Can I use the ISO154X to dereference the I2C port referenced to the middle ground? If not, can somebody suggest any other alternative on how to do this?

Thanks,

Carlos