Other Parts Discussed in Thread: LMH0307, LM3100
We have a design that uses the LMH0307 SDI cable driver. On our second batch of boards we have discovered that the SDI output pin (pin 12) on some of the cable drivers is shorted to the 3V3 supply rail. At first we assumed this was an assembly error, but further investigation shows that this pin (and associated PCB trace) are not adjacent to any 3V3 traces. In order to isolate the issue, we then removed the passive components on this trace, leaving only the LMH0307, and the short remains. So the short must be coming from the LMH037 itself.
In our last batch of boads we have 6 boards which are OK, and 4 boards with this issue. The short was discovered on the boards when they were powered up for the first time, directly from manufacture.
So my question is, what could cause this short between LMH0307 pin 12 and the 3V3 supply?
Adam