This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84 Questions

Guru 16770 points

Other Parts Discussed in Thread: SN65DSI84

Hi

We want to make the conversion like following.

[INPUT MIPI-DSI]
3 Lane
Clock : 486MHz
RGB : 8:8:8 bit
Data : 1024 x 768

[OUTPUT LVDS]
2 Link
RGB : 24bit VESA format
LVDS Clock : 54MHz

Could you advise me for the following?

1. Is it possible to carry out above conversion by SN65DSI84?
2. We don't have REFCLK. Is it OK?

regards