Other Parts Discussed in Thread: TUSB1210
Hi all,
I have placed an FPGA between Motherboard and Pendrive @ USB2.0 interface via Device and Host side TUSB1210.
Now I want to extract the payload from the motherboard, process the data and transfer to the pendrive. Before I could do that I am stuck at a much earlier phase.
My pendrive does enumerate, gets formatted, written, read on WIN-XP machine but does not enumerate on WIN-7 m/c.
When I see on the chipscope, I find that as the INQUIRY command comes from the HOST, pendrive replies using NYET that is transferred to HOST. But then host sends a PING command.
Is sending PING command a normal phenomenoon WIN -7 m/c. Or is it that HOST did not receive the reply in right time from the pendrive VIA FPGA.
Any hint on this will be highly grateful!!!
Regards