This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947 keeps streaming out some data when its input switch off



Hello,

I'm working on a repeater board that consists of one DS90UB948 deser. and one DS90UB947 ser. These two are connected 1:1 so D0 --> D0...D7-->D7 and CLK --> CLK (according to datasheet)  VIDEO_SOURCE_SER ---> DESER1 ----> SER -----> DESER2
 The board works good, the signal goes through, video after repeater is OK, but I have some problem. When the source of a signal is switched off, the deserializer (DESER1) stops generating CLK and data (correct), but the serializer still streams out a signal down to the link. When I connect another board to the output of the first, I see that its deserializer (DESER2) catches CLK signal and is LOCKed. The problem is that the serializer (SER) still streams a CLK with zero data in spite of its input (DESER1) streams nothing.

I tryed to set SOFT_SLEEP register in the serializer, but it did not help.


 My question:

Is that correct behaviour?

How can I detect that the source of the signal is switched off, when I have still LOCK signal on second deser asserted?

Thank you for any ideas.


Ondra