Other Parts Discussed in Thread: TPS65982
Hi all,
I've tried the TPS65982/86 successfully with a real USB-C host. But it still does not work correctly if using a normal USB host.
The problem is that the USB host does not support CC configuration. So when I check the log file (by using read_register Python script), it says DataConnection is disconnected (Data Status 0x5f), thus I think the USB Mux is not enable.
Guess I have to control the register of TPS65982/86 directly. Is it okay to manually control the "0x28 System Configuration" register, bit 34-33 USBPath to enable "USB RP path"?
Or is there other way to activate the USB Mux in this case?
Attached is the log file (read_register) and the Config file I'm using. Pls help to check and advise. Thank you all.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/138/Test1.7z