This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RXAUI to XFI Transceiver



Hello,

My customer is looking for an RXAUI to XFI transceiver.  Do we offer such a device?  I could not find a match on the web or ESP.

Thanks,

Dan

  • Hi Dan,

    XFI is a 10.3125 Gbps 64/66 bit encoded serial data.

    RXAUI is 6.25 Gbps 8b/10b encoded serial data.

    RXAUI is designed to allow 2 lanes of 6.25 Gbps data be able to handle one lane of 10Gbe.  For standard XAUI at 3.125 Gbps for lanes are needed.

    I am not aware of any TI SVA SerDes devices which can translate between these two specifications.

    Regards,

    Lee