Other Parts Discussed in Thread: TPS65982, TPS6598X-CONFIG
Hello,
I have some doubts in this TPS65982.
1)Can this device can be operated in Device Mode?If Yes Please provide the Reference schematic in Device Mode.
2) I have two Type-C connectors one is acting as Host and another one acting as Device.Two TPS65982 Devices should be used to generate the CC and SBU and VCONN signals?One TPS65982 acting as Host for the Device Type-C Port and another TPS65982 acting as Device for Host Type-C Port.Is it right?
3) Is this IC is used in PC or Laptop Interface for Type-C.
With Regards,
Suneetha.V