This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS3243EIRHBR About 25pin



Hi,

My customer is using TRS3243EIRHBR.
He has a question about 25pin which is N.C pin.

Can customer input 3.3 voltage to 25pin?

N.C.is showed as "Not internally connected" in datasheet,
I think that there is not problem for 3.3V input to 25 pin.

Customer wants to use this device as replacement of ISL3243EIRZ.

Best regards,
Shimizu