Other Parts Discussed in Thread: TUSB2077A
Designed in the 2077A which seemed straight forward and populated minimal components like crystal, LDO, reset controller, etc... just to get basic powerup of the device confirmed. Double and triple checked the assembly and pretty sure the design is wrong. HUBCFG is aways low so the chip isn't configured on powerup. This is as basic as it gets, with no eeprom, downstream ports powered with separate supply, etc. The plan is to slave another 2077a of the root controller for 12 total ports and I can't even get the 1st controller running. All static voltages on the pins are fine. Would be nice to see any type of activity on some output likes, but nothing is happening on any lines except the xtal inputs Attached is the schematic and and feedback would be appreciated.
Thanks
Phil16240.pdf