[ DS90UB914A-Q1 ] Not to use GPIO
Hi Expert,
It seems that there are no pull-up/down resistors in GPIO[1:0] and GPIO[3:2] pins. If we don't use these pins, can these be left open?
* No GPIO function used between 913A and 914A
* No multiple camera frame sync
* No external reference clock usage
* No BIST
It's great help if you can let me know other things I need to take care.
Thanks,
Ken
Other GPIO related reference.
DS90UB913A GPIO
e2e.ti.com/.../1321554