This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using 2 TPS65982 IC for two Type-C Connectors

Other Parts Discussed in Thread: TPS65982

Hello,

In one of my project, I want to use two Type-C connectors one Type-C connected to Host and and another Type-C connected to Device.

The Host Type-C will be acting as DFP and Device Type-C acting as UFP.

I am using two TPS65982 Devices to implement the USB-PD between Host and Device.

Can I use I2C Ports to communicate between them?

Can I transfer the Power of 100W (20V,5A) from Type-C (Host) to another Type-C (Device) with the below diagram?

Can I take the VBUS voltage from Type-C(5V or 20V) to PP_HV and PP_EXT pins,without giving external voltages to these pins?

TPS65982.docx

Waiting for feedback

With Regards,

Suneetha.