Other Parts Discussed in Thread: TPS65982
Hello,
In one of my project, I want to use two Type-C connectors one Type-C connected to Host and and another Type-C connected to Device.
The Host Type-C will be acting as DFP and Device Type-C acting as UFP.
I am using two TPS65982 Devices to implement the USB-PD between Host and Device.
Can I use I2C Ports to communicate between them?
Can I transfer the Power of 100W (20V,5A) from Type-C (Host) to another Type-C (Device) with the below diagram?
Can I take the VBUS voltage from Type-C(5V or 20V) to PP_HV and PP_EXT pins,without giving external voltages to these pins?
Waiting for feedback
With Regards,
Suneetha.