Other Parts Discussed in Thread: ALP
I am from DLP group in Dallas using the 925 Serializer EVM with 948 Deserializer EVM and we have our Automotive EVM hooked up to 948 on both the OpenLDI and I2C interfaces.
The Video is working fine however we are not able to setup the I2C Remote Slave. Here is the configuration.
Laptop (ALP App) <-> 925 <-> 948 <-> DLP Automotive EVM
Basically the Laptop is connected to 925 EVM and the Remote Slave is DLP EVM. The I2C addresses for 925 is 0x18 (default), 948 is 0x58 (default) and our DLP EVM is 0x36.
It is not clear how to configure the I2C on the Remote Deserializer to behave as the Master Proxy for the DLP EVM. I have setup the Remote Slave ID address on the Serializer correctly
and also setup the enabled pass-thru on both 925 Serializer and 948 Deserializer.
There is an App Note SNLA131A however it does not have clear instructions or an example. Could you provide the exact steps to setup this correctly.
I can be reached at 214-384-5602.
This is an important task for us so any help is much appreciated.
Regards,
Balaji Srinivasan
214-384-5602